Question
ST MC Workbench + ST FOC library
Posted on July 14, 2013 at 01:41
Hi, as I couldn´t get any ifn003v1 board, I bought an EVAL6230QR with an stm32f4discovery, and I´m trying to get them work together with the ST FOC library the ST MC Workbench and a MAXXON motor (EC-max 283833).
I´m trying to run the demo code, the one that starts and stops the motor repeatedly. But it turns out that it resets because of a fault. by debugging I could find that the error is defined as MC_SPEED_FDBK, and I was trying to find out why.
Is the St MC workbench set wrong? I´m wiring something wrong? I will appreciate any help to set the parameters correctly. Thanks in advance,Best Regards