2022-03-31 07:55 PM
Hello, I am using L6205D013TR on our PWB.
I would like to use L6205D instead of L6205D013TR, but
I could not find the difference between L6205D and L6205D013TR on their Data sheets. Please tell me the meaning of "013TR". It's just a difference of the pack?
Solved! Go to Solution.
2022-04-01 12:51 AM
Hello @�?� 西尾 and welcome to the ST Community.
I confirm that the only difference between the two ordering codes is the packing type.
L6205D013TR is L6205D delivered in Tape&Reel 13"
L6205D is delivered in Tube
Please click on the 'Select as Best' label if I fully answered to your question.
2022-04-01 12:51 AM
Hello @�?� 西尾 and welcome to the ST Community.
I confirm that the only difference between the two ordering codes is the packing type.
L6205D013TR is L6205D delivered in Tape&Reel 13"
L6205D is delivered in Tube
Please click on the 'Select as Best' label if I fully answered to your question.