2017-02-10 06:32 AM
Dear all, I need to know the range of the parameters (load capacitance, series resistance) allowed by the STPM32 IC.
I didn't find these values neither on the datasheets nor on the applications.
Can you help me?
Thanks in advance,
Franco.
#crystal #parameters #stpm322018-05-29 06:24 PM
As with Franco above, we'd like to know the range of allowed crystal parameters by the STPM32:
1. Load capacitance
2. Series resistance
3. PPM range
4. Internal pin capacitance
Thanks!
Cheers,
Angelo
2023-07-23 02:36 PM
As above I too require these details.