cancel
Showing results for 
Search instead for 
Did you mean: 

Crystal parameters for STPM32.

Franco Zampicinini
Associate II
Posted on February 10, 2017 at 15:32

Dear all, I need to know the range of the parameters (load capacitance, series resistance) allowed by the STPM32 IC.

I didn't find these values neither on the datasheets nor on the applications. 

Can you help me?

Thanks in advance, 

Franco.

#crystal #parameters #stpm32
2 REPLIES 2
Angelo M
Associate
Posted on May 30, 2018 at 03:24

As with Franco above, we'd like to know the range of allowed crystal parameters by the STPM32:

1. Load capacitance

2. Series resistance

3. PPM range

4. Internal pin capacitance

Thanks!

Cheers,

Angelo

BartW
Associate

As above I too require these details.