2003-06-11 6:24 AM
2011-05-17 1:16 AM
I am using the st72141k for a motor controller. In order for my stop motor routine to work correctly, I have to constantly reset the
watchdog timer in the shut down routine. Here is the code: .stop_motor ld A, #$00 ; set MOE bit to 0 ld MCRA, A .stall ld A, #$7F ld WDGCR, A ; reset watchdog timer ld A,#$FF ; turn light off ld PBDR,A call wait_500ms ; 500ms delay ld A,#$FB ; turn light on ld PBDR,A jp stall ; repeat forever Now, the code above will stop the motor, but the LED will not flash as it should. I can run the flash code (turns output pin on/off that is tied to the negative voltage side of the LED) else where in the program and the LED will flash, but when it is in this stall loop it never works. The wait_500ms is just a counter that counts for ~500ms. I even have that reset the watchdog as the watchdog timeout is ~98ms. If I do not reset the watchdog then the motor stops momentarily and then tries to restart repeadly and usually at that point a driver fails. Any ideas? Thanks for the help.2011-05-17 1:16 AM
first you need to be servicing the watchdog in your wait_500ms routine...
then you need also to wait 500 ms before turning the LED off again otherwise the time off will be so short that you won't be able to see it...