2019-02-27 05:35 AM
Dear All,
I changed the MOSFETs on IHM08M1 to STP110N7F6 and modified the settings of dead time of Driver and Mosfet in MC work bench. But the BLDC can't run well(it doesn't reve-up often) . The manual of MC work bench only indicate user to modify mosfet setting according to electric characteristic. What else setting should I adjust? (Before I changed the mosfet, my BLDC works fine).
Thanks .
2019-03-06 11:27 PM
Hi,
could you share some screenshot about the motor current on the three phases ? Did you try to reduce the acceleration during the startup changing the speed ramp generation (see Start-up parameters on WB tool) ? If the MOSFETs are correctly mounted I don't think there are issues on HW part.
Regards.
Giuseppe