cancel
Showing results for 
Search instead for 
Did you mean: 

can I use wireless charging IC in a resonant frequency of 13.56HZ?

helpm
Associate

I want to buy a wireless charging IC like STWBC86JR, but the data sheet says that it should be within the standard frequency of 110kHZ to 205kHZ, so can't I use it with a resonant frequency of 13.56MHz? Is there an IC available on that frequency? Is there a way to design an additional circuit and communicate at that frequency?

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @helpm, to the community!

The STWBC86 is a Qi power transmitter, i.e. it is set to the frequency range 100...205kHz defined in the Qi standard.

There is currently no comparable power transmitter available for 13.56MHz, but there are possibilities to communicate and to do wireless charging with NFC.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.