2014-09-28 7:21 AM
Gigi:
I'm in the Bus Voltage Sensing parameter settings of Workbench when the input voltage is 24V, I am a divider resistor R1 = 51K R2=1K, how to calculate excuse me my Bus voltage sensing network partitioning factor?  Best Regards  Jacky2014-09-29 12:20 AM
Ciao Jacky
Usually the Bus Voltage Sensing is done with a simple voltage divider. Considering the one explained you have to compute the Vin/Vout ratio that depends only on the resistors network: Vin is the DC bus voltage and Vout is the input of the ADC of the micro. In your case, I assume that the R2 is between Vout and ground. Bus Voltage Sensing = (51K + 1K)/(1K) = 52 This mean that you are scaling 52 times the DC bus voltage -> 0.46V to ADC (exploiting small part of the range. Maybe the petitioning factor can be improved). Ciao Gigi2014-09-29 9:29 AM
Thank you, the problem is solved.
2014-09-30 12:54 AM
Hi Gigi,
I would like to comment on a possible improvement on that configuration item. I also stumbled on this for a moment because - on other locations, the tool asks for a gain (for example, current sensing), which is more straight forward in my opinion. - for the bus voltage, I can only enter an integer value. In my design, the attenuation factor isn't. - in the resulting header file, this number is indeed converted into a (floating point) gain. Regards Frank