cancel
Showing results for 
Search instead for 
Did you mean: 

Boost LED Driver

ammar
Associate
Posted on July 03, 2017 at 12:13

We are using LED6001 LED Driver in a Flasher.

The problem is when the input is less than 10.5V it works O.K but when the input is more than 10.5V the LED current reduces to almost 10mA or shuts down. The Problem is same with 6LEDs at the O/P and 12LEDs at the O/P. We have also tried shifting the OVP much above the O/P required volatage, but still this problem exists.

Please help us to resolve the problem.

 Please find the updated schematic.

#boost-led-driver #led6001 #led-driver
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ammar
Associate
Posted on July 12, 2017 at 09:33

I think the problem is with Input current sensing and COMP R-C values, could anyone help me to sort out it.