cancel
Showing results for 
Search instead for 
Did you mean: 

Are the pins of this high side driver ( VND5E160AJ-E ) correct ? The datasheet show that 2th input pin controls 10th and 11th output pins but it is not correct. The 3th input pin controls 10th and 11th output pins. Is this IC reliable ?

bülent küpeli
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luigi INNACOLO
Associate II

Hello,

The VND5E160AJ-E is a dual channel high side drive, so there are only two INPUT pins, and each of the INPUT controls the relevant OUTPUT. The other input pin, called CS_DIS, allows to disable the diagnostic feedback in case the device is used in parallel configuration (two or more devices in parallel, sharing the same sense resistor).

The device is reliable, considering it is automotive grade, AEC-Q100 qualified.

Best regards,

Luigi

View solution in original post

1 REPLY 1
Luigi INNACOLO
Associate II

Hello,

The VND5E160AJ-E is a dual channel high side drive, so there are only two INPUT pins, and each of the INPUT controls the relevant OUTPUT. The other input pin, called CS_DIS, allows to disable the diagnostic feedback in case the device is used in parallel configuration (two or more devices in parallel, sharing the same sense resistor).

The device is reliable, considering it is automotive grade, AEC-Q100 qualified.

Best regards,

Luigi