Hello,ST usually provides FIT rate data. I would recommend to contact your local sales office for more information at the following link: https://www.st.com/content/st_com/en/contact-us.html
Hello,The VND5E160AJ-E is a dual channel high side drive, so there are only two INPUT pins, and each of the INPUT controls the relevant OUTPUT. The other input pin, called CS_DIS, allows to disable the diagnostic feedback in case the device is used i...
Posted on June 25, 2018 at 16:25Hello Matteo,paralleling VN7003ALH devices is not recommended only in case of inductive loads. For all other cases, further information can be found in the 'VIPower® M0-7 standard high-side drivers hardware design gui...