2004-11-07 8:49 PM
'Alternate Z Sampling' daughter board
2011-05-17 1:17 AM
I've started working with the ST7MC2 Starterkit to develop a BLDC application. Up to now I'm very satisfied with the performance of the ST7MC2.
Because I have to realize a high speed application, I want to to work with the standard Z detection method with external voltage dividers. The manual refers to AN1946 to calculate the voltage dividers, but I can not find AN1946. Does anybody know where to find AN1946 or knows how to calculate the voltage dividers and where to mount the resistors on the 'Alternate Z Sampling' daughter board ? Ludwin2011-05-17 1:17 AM
Hello Ludwin,
as I know AN1946 is not available yet, please be free to contact me directly in order to solve this matter. Luca Defend http://www.softecmicro.com