Posted on May 17, 2011 at 10:19I have apadpted the BLDC Sensorless Motor Library to the ST7FMC1. It's working fine. The library is using Timer B. But according to the ST7FMC datasheet the ST7MC1 isn't equipped with Timer B. A check with the debugger...
Posted on May 17, 2011 at 10:17I've started working with the ST7MC2 Starterkit to develop a BLDC application. Up to now I'm very satisfied with the performance of the ST7MC2. Because I have to realize a high speed application, I want to to work with...