Posted on May 17, 2011 at 10:17Hello Ludwin, as I know AN1946 is not available yet, please be free to contact me directly in order to solve this matter. Luca Defend http://www.softecmicro.com
Posted on May 17, 2011 at 10:171) ST7MC1 has a small RAM, 384 bytes only, are you sure that it is enough? 2) ST7MC1 has a just 8K of FLASH memory, can you fit your project (although shortened) into the MCU? 3) PWM doesn't work on MCO outputs, but I ...
Posted on May 17, 2011 at 10:17Quote:On 2004-07-12 18:45, kojote wrote: Is it true, that there is no SW, which could be connectet throu a cable to the target's ISP connector, and does the same job the board does. Is it because the board does it fast...
Posted on May 06, 2005 at 05:44The problem could be caused by the Watchdog. You know that ST7FLITE0 device has Option Bytes to set some of the device features. If you use DataBlaze you can issue an Erase command then goto the Option Bytes Window and...
Posted on May 01, 2005 at 19:32As you can find on SofTec Microsystems FAQ page: This happens when your target device doesn't feature the on-chip debug module. In this case, step commands are not executed in real time, for a series of reasons which a...