Skip to main content
KOksa.1
Visitor II
Apr 8, 2020 10:48 AM UTC
Question

ı am reading wrong Current value at STC3100. I need help to get right Current Value.

Hi,

I attach my Power Side of Project Schematic.

I will use STC3100 IC at my circuit. I will use Li-ION AA type Cell in my circuit and I charge my cell externally on charge device. So ı don't use STC3100 while charge status monitoring. I will use STC3100 only monitoring available charge status. So, I applied referance schematic at datasheet ot STC3100 and I used 10mili ohm between GND and (-) of Cell. And also I developed my code and ı am sending debug LOG at below.

My first question is this: I pull approximately 100mA at my circuit but I read 9000mA (9 Amper) from Current registers. At document it says Current Register is 14 Bit (Bit-13 is sign and Bit 0-12 is data) and I read convert only 12 data bit to Decimal and use it inside formula "STC3100_Application_Doc.pdf" page 8. Formula is "current (mA) = current_code* 11.77 / Rsense (mΩ)" But the result is approximately 9000mA. So at which point I have fault, can you inform me?

REG_CHARGE_LOW: 248;REG_CHARGE_HIGH: 127 --- CHARGE: 21864.1093 mA.h

REG_COUNTER_LOW: 113;REG_COUNTER_HIGH: 0 --- COUNTER: 113.0000

REG_CURRENT_LOW: 255;REG_CURRENT_HIGH: 30 --- CURRENT: 9304.1845 mA (????)

REG_VOLTAGE_LOW: 184;REG_VOLTAGE_HIGH: 5 --- VOLTAGE: 3559.9599 mV

REG_TEMPERATURE_LOW: 184;REG_TEMPERATURE_HIGH: 0 --- TEMP: 23.0000 °C

REG_CHARGE_LOW: 247;REG_CHARGE_HIGH: 127 --- CHARGE: 21863.4394 mA.h

REG_COUNTER_LOW: 123;REG_COUNTER_HIGH: 0 --- COUNTER: 123.0000

REG_CURRENT_LOW: 255;REG_CURRENT_HIGH: 30 --- CURRENT: 9304.1845 mA (????)

REG_VOLTAGE_LOW: 184;REG_VOLTAGE_HIGH: 5 --- VOLTAGE: 3559.9599 mV

REG_TEMPERATURE_LOW: 185;REG_TEMPERATURE_HIGH: 0 --- TEMP: 23.0000 °C

Also, to monitoring Li-ION cell (1 Cell), what is your application suggestions? I want to power down my circuit when Cell Voltage is 3.0V at Min. But beucause circuit load pulls current, this voltage value will seem lower than 3.0V. So, is there a reference application steps which you will suggest?

Thanks.

This topic has been closed for replies.