what is Keil builtin Function/command to set the Prescaler for stm32f103 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-30 8:43 AM
reading the reference manual of stm32f103, i came to know that ADC prescaler is set using RCC_CFGR in keil.
hence in keil
xxxxxxxxxxxxxxxxxxx=RCC_CFGR_ADCPRE_DIV2;
i dont know what to put at the place of xxxxxxx in Keil ?
as in case of stm32f4 i know
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
but it does not work for stm32f103
can you help me please regarding this.
thanks
- Labels:
-
ADC
-
Keil
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-30 10:22 AM
ADC clock configuration is separate from other ADC configuration for F103.
The SPL had this function:
/**
* @brief Configures the ADC clock (ADCCLK).
* @param RCC_PCLK2: defines the ADC clock divider. This clock is derived from
* the APB2 clock (PCLK2).
* This parameter can be one of the following values:
* @arg RCC_PCLK2_Div2: ADC clock = PCLK2/2
* @arg RCC_PCLK2_Div4: ADC clock = PCLK2/4
* @arg RCC_PCLK2_Div6: ADC clock = PCLK2/6
* @arg RCC_PCLK2_Div8: ADC clock = PCLK2/8
* @retval None
*/
void RCC_ADCCLKConfig(uint32_t RCC_PCLK2)
{
uint32_t tmpreg = 0;
/* Check the parameters */
assert_param(IS_RCC_ADCCLK(RCC_PCLK2));
tmpreg = RCC->CFGR;
/* Clear ADCPRE[1:0] bits */
tmpreg &= CFGR_ADCPRE_Reset_Mask;
/* Set ADCPRE[1:0] bits according to RCC_PCLK2 value */
tmpreg |= RCC_PCLK2;
/* Store the new value */
RCC->CFGR = tmpreg;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 5:27 AM
thanks for your reply,
i write you code below, the last 2 lines give me error, the commands that you told me RCC_PCLK2_Div2: ADC clock = PCLK2/2 is not working in this way.... the way i am writing the code,
i hope you can understand
#include <stdio.h>
#include "stm32f10x.h" // Device header
#include "GPIO_STM32F10x.h" // Keil::Device:GPIO
#include "stm32f10x_adc.h" // Keil::Device:StdPeriph Drivers:ADC
#include "stm32f10x_rcc.h" // Keil::Device:StdPeriph Drivers:RCC
#include "stm32f10x_gpio.h" // Keil::Device:StdPeriph Drivers:GPIO
void ADC_Configuration(void);
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
int main () {
unsigned int j;
//----------------------------------------------------------------------------------------
// Software triggered, dual, simultaneous sampling
//----------------------------------------------------------------------------------------
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_ADC2, ENABLE); //Enabling ADC1 and ADC2 clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB, ENABLE); //Enabling GPIOA and GPIOB Clock
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2; //Analog voltages to be measured are connected to pins 1 and 2 of port A,
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; //Analog input mode for ADC
GPIO_Init(GPIOA, &GPIO_InitStructure); // calls the function to actually configure the port A.
//ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
//ADC_CommonInitStructure.ADC_Mode = ADC_DualMode_RegSimult;
ADC_InitStructure.ADC_Mode=ADC_CR1_SCAN;
RCC_PCLK2_Div2:ADCclock = PCLK2/2; // ----->>> do not accept colon
RCC_PCLK2_Div2 = RCC_CFGR_ADCPRE_DIV2;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 5:55 AM
thanks for your reply
i think you are using '' Pro*C Embedded SQL '' for your code. am i right ?
i am not familiar with it, i have posted my code written in embedded C below in another post, if you get an idea please reply me.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 6:14 AM
You could just use the function, for example:
RCC_ADCCLKConfig(RCC_PCLK2_Div2); // set ADC clock to PCLK2 / 2
I'm not familiar with "Pro*C Embedded SQL", my project is just using embedded C and the ST standard peripheral library, which it appears you are also using.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 6:33 AM
thanks again,
it's okay that if i use for prescaler
RCC_ADCCLKConfig(RCC_PCLK2_Div2); // set ADC clock to PCLK2 / 2
but there is another function in Keil like ''RCC_CFGR_ADCPRE_DIV2''
can you please tell me , how are they related to each other, for example in which case i can use
RCC_CFGR_ADCPRE_DIV2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 6:57 AM
To change the ADC clock divider, the appropriate bits of RCC->CFGR need to be set to the desired value, that's what RCC_ADCCLKConfig() does.
As you can see from the definitions, RCC_CFGR_ADCPRE_DIVx is equivalent to RCC_PCLK2_Divx; you could use either (many people would prefer to use function arguments as the function documentation instructs, but the hardware only cares about numbers).
#define RCC_CFGR_ADCPRE_DIV2 ((uint32_t)0x00000000) /*!< PCLK2 / 2 */
#define RCC_CFGR_ADCPRE_DIV4 ((uint32_t)0x00004000) /*!< PCLK2 / 4 */
#define RCC_CFGR_ADCPRE_DIV6 ((uint32_t)0x00008000) /*!< PCLK2 / 6 */
#define RCC_CFGR_ADCPRE_DIV8 ((uint32_t)0x0000C000) /*!< PCLK2 / 8 */
#define RCC_PCLK2_Div2 ((uint32_t)0x00000000)
#define RCC_PCLK2_Div4 ((uint32_t)0x00004000)
#define RCC_PCLK2_Div6 ((uint32_t)0x00008000)
#define RCC_PCLK2_Div8 ((uint32_t)0x0000C000)