STM32L0 Problem with EXTI handler on platform.io & arduino framework
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 5:51 AM - last edited on ‎2025-04-07 6:29 AM by Andrew Neil
Hi,
I'm using a STM32L031K6 with platform.io & arduino framework. I know this forum is not relevant to platform.io or arduino, but most of my code is with LL drivers which should change nothing (but maybe ?).
First, i don't understand the IRQn. I'm using PB1 as input interrupt on rising, it's on line 1, so to start, it should be :
NVIC_EnableIRQ(EXTI0_1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
//as refered :
EXTI0_1_IRQn = 5, /*!< EXTI Line 0 and 1 Interrupts
But the interrupt work only if i enable EXTI2_3_IRQn. I don't get it, and in example EXTI_ToggleLedOnIT for NUCLEO-L073RZ, there is the same +1 on IRQn.
So, change made, and i can see the change of the interrupt on IEXTI->PR, depending on the rising on PB1. the problem is the call back function. On STM32 IDE, there is a *_it.h/c which don't exist on platform.io. Maybe the point come here.
First, i wanted to change the function handler using :
void IRQ_Module_0(void) {;}
NVIC_SetVector(EXTI2_3_IRQn, (uint32_t) &IRQ_Module_0);
But it seems to do nothing as the adress return by NVIC_GetVector stay the same. Or maybe i forgot something.
Second, i try to figure out with the defaut handler (which was hard to find, documentation is not clear) :
/**
* @brief This function handles external line 2 to 3 interrupt request.
* None
* @retval None
*/
void EXTI2_3_IRQHandler(void)
{
uint32_t pin;
for (pin = GPIO_PIN_2; pin <= GPIO_PIN_3; pin = pin << 1) {
HAL_GPIO_EXTI_IRQHandler(pin);
}
}
// ->
void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)
{
/* EXTI line interrupt detected */
if (__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
HAL_GPIO_EXTI_Callback(GPIO_Pin);
}
}
// ->
__weak void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(GPIO_Pin);
/* NOTE: This function Should not be modified, when the callback is needed,
the HAL_GPIO_EXTI_Callback could be implemented in the user file
*/
}
with a new function :
extern "C" void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {;}
And get an error :
test.cpp:(.text.HAL_GPIO_EXTI_Callback+0x0): multiple definition of `HAL_GPIO_EXTI_Callback'; .pio/build/nucleo_l031k6/SrcWrapper/src/stm32/interrupt.cpp.o:interrupt.cpp:(.text.HAL_GPIO_EXTI_Callback+0x0): first defined here
But it is defined as __weak
There is also in interrupt.cpp some :
void EXTI0_IRQHandler(void)
{
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);
}
Finally, i'm totally lost. Did i make some missunderstanding ? Or maybe it is relative to platform.io ?
I search for some same error and didn't find it.
Some help would be appreciate.
Thx in advance,
Solved! Go to Solution.
- Labels:
-
GPIO-EXTI
-
STM32L0 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 11:30 AM
So, i add __weak to EXTI0_1_IRQHandler and EXTI1_2_IRQHandler inside framework-arduinoststm32\libraries\SrcWrapper\src\stm32\interrupt.cpp
It's dirty, but fastest way to solve it. I need to go to stmcube framework, but can't find a "all in one" LL (or HAL) printf library. Actually, i don't want to make my own.
Thanks,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 6:31 AM
@Frog wrote:I know this forum is not relevant to platform.io or arduino, ,
Indeed - maybe better to try here: https://www.stm32duino.com/
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 7:22 AM
In fact, there is a mistake cause of VSCode when i was looking to the function
__weak void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
Refer to the hal_gpio library, but in fact, it is declared inside interrupt.cpp
/**
* @brief This function his called by the HAL if the IRQ is valid
* @PAram GPIO_Pin : one of the gpio pin
* @retval None
*/
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
uint8_t irq_id = get_pin_id(GPIO_Pin);
if (gpio_irq_conf[irq_id].callback != NULL) {
gpio_irq_conf[irq_id].callback();
}
}
But arduino framework or not, that change nothing about the EXTI2_3_IRQn for line1 and the problem of NVIC_SetVector which are from LL drivers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 11:30 AM
So, i add __weak to EXTI0_1_IRQHandler and EXTI1_2_IRQHandler inside framework-arduinoststm32\libraries\SrcWrapper\src\stm32\interrupt.cpp
It's dirty, but fastest way to solve it. I need to go to stmcube framework, but can't find a "all in one" LL (or HAL) printf library. Actually, i don't want to make my own.
Thanks,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 11:46 AM
@Frog wrote:i add __weak to EXTI0_1_IRQHandler and EXTI1_2_IRQHandler inside framework-
If you're adding it, don't specify the __weak - that's saying, "this is just a default; could be overwritten"
If that's solved the issue, please mark the solution:
https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
@Frog wrote:can't find a "all in one" LL (or HAL) printf library. Actually, i don't want to make my own.
Thanks,
Not sure what you mean by that?
But maybe this helps:
If not, please start a new thread with the new question.
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-07 11:55 AM
I mean, it was :
void EXTI0_1_IRQHandler(void)
It become
__weak void EXTI0_1_IRQHandler(voir)
So i can overwrite it. It's not really a solution because it change the main library, so on next update i will need to change it again. In fact, i don't understand why its not "__weak" by defaut so the user can choose to overwrite or not.
I mean a .c/.cpp/.h to include and it works, but your solution looks not to hard to make it working. Thanks :)