2025-12-05 8:03 AM - last edited on 2025-12-05 8:48 AM by Andrew Neil
We repair Fire Alarm Panels, and I have a known good chip PSD813F1A that I can read and save the data but when I program the blank device it will program but then gives me a verify error and it doesn't function in the panel. I'm using the Logical devices XPRO programmer with the proper adapter DX2052 (PLCC). It is listed in the program's library so that's not the issue. Not sure if there's a source to properly program this device or do I need special programming software and programmer to accomplish this. Any help will be amazing!!
Thanks for allowing me post here.