2021-04-06 9:04 AM
2021-07-01 11:52 AM
Please help me fix the error:
Failure at line:6 in 'Target Software Scripts'. Please edit debug configuration setting.
Cannot convert between character sets 'CP65001' and CP1252'.
Thanks a lot!!!
2021-07-01 1:22 PM
Do the two machines have different keyboard settings?
2021-07-01 1:39 PM
Hello @hroze.1 ,
This seems like an encoding issue. Converting the file encoding might help you. Funnily enough, and because the file fits within Latin-1, you would be able to do that using Notepad++ by selecting the ANSI encoding and then saving the file:
Hope this helps.
Best regards,
@SBEN .2
2021-07-03 11:58 PM
I have the same problem
An old computer works without problems A new computer has the problem
I would appreciate if you could share with me how you solved the problem
2021-08-12 7:20 AM
I had the same problem, the problem is not related to Atollic itself, we need to diable utf8 for worlwide language in Windows
2024-01-29 6:30 AM
You are a genius. Thanks.
Ondrej