2025-04-02 4:45 AM
Hii, I want to update the firmware of my STM32H723ZGT6 microcontroller. Here, I want to send firmware file from server to W5500 Wiznet IC then I want that this firmware should load in to the microcontroller flash and it should update the program so can anyone help me with this??
Solved! Go to Solution.
2025-04-02 5:00 AM
Hello @Aries16 and welcome to the community,
W5500 seems to be a SPI/Ethernet bridge.
If you intend to use the SPI bootloader, you have to take care about the bootloader protocol over the SPI:
Refer to this application note.
You need to handle the Boot pin and the reset pin of the STM32H7.
2025-04-02 4:55 AM - edited 2025-04-02 7:01 AM
"OTA" = Over The Air.
But a W5500 is a wired ethernet device.
The STM32H723ZGT6 already has ethernet built-in - so why would you add a W5500 ??
Anyhow, what you need is a Bootloader.
PS:
On Bootloaders for STM32:
https://community.st.com/t5/stm32-mcus/why-do-we-need-a-bootloader-in-a-microcontroller/ta-p/49446
https://community.st.com/t5/stm32-mcus-embedded-software/official-stm32-bootloader/td-p/591959
STM32H7 specifically:
2025-04-02 5:00 AM
Hello @Aries16 and welcome to the community,
W5500 seems to be a SPI/Ethernet bridge.
If you intend to use the SPI bootloader, you have to take care about the bootloader protocol over the SPI:
Refer to this application note.
You need to handle the Boot pin and the reset pin of the STM32H7.