NRF24301 working library
Hello,Please suggest me some library for NR24L01 which is prefectly working. It should based on C language. I search few posts but many libraries are not working as I could see in comment section. Regards,Manoj Hiwarkar
Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.
Hello,Please suggest me some library for NR24L01 which is prefectly working. It should based on C language. I search few posts but many libraries are not working as I could see in comment section. Regards,Manoj Hiwarkar
Hello,We are facing COO issues with almost all STM32G4 and H5 MCUs. The website/invoice says COO is non china and when we actually get the products, the chip marking is CHN. When enquired, STMicro team bluntly emails saying CHN is not China. After 20...
I am having a hard time figuring out working with the STM32-E407 which is built on STM32F407ZGT6 MCU. I also brought an ARM-USB-TINY-H as it was recommended in its documentation. How and where do I start ? Say I want to interface this board with a ra...
Hello everyone,for a project at the university i have to programming an nextion display with a stm32f401re or a stm32g474re. (i can choose between them, i have both here). My problem is that i have configurate the display with the nextion editor. Th...
I'm attempting to get started with the Morse Micro MM8018-EKH05 (STM32U585VIT6 controlled) and pair it with their HaloLink1 router. I am following their MM8108-EKH05 used guide user guide section "5.2 Build and Run Example Applications." I have load...
Hello,I’m working on a design using the STM32H750IBTx (LQFP176) running at 400 MHz with FreeRTOS, and I’ve encountered a strange intermittent issue with the display that only appears after long periods of operation.Problem Description:After about 30–...
Dear Sir , Kindly Help In Writing Program for PFC Boost Control. As i have worked on making an power supply with Below Specification Details :Input Voltage : 1 to 20 VAC(Variable)Input Current : 3Amps (Constant)We Require : Output Voltage : 30VDCOutp...
Dear STM32 Support Team,Good afternoon.I am currently working on an STM32H7-based project using the Cortex-M7 core. The firmware is compiling and flashing successfully without any errors. However, I am facing an issue during live debugging — the brea...
Hello, everyone. Can anyone tell me how? I want to do something while STM erases a sector, Since it is STM32F401, it takes too long to erase a sector. What can be the best solution?