cancel
Showing results for 
Search instead for 
Did you mean: 

LVGL with LCD display using LTDC

b1aze
Associate II

Hi all i used LTDC hardware inside the STM32f429 discovery board to drive an external 24 bit RGB display in 16 bit mode . full GUI is designed in LVGL library , I was able to build it and flash it. I got the output on the display but with few issues .

1.the update speed of the GUI elements are way too slow , so I cant update it real time

2.I am not getting a precise output .some pixels are lost, 

3.can I change the horizontal animation happening when changing the screen

4.How to use DMA2D to copy pixel data to framebuffer

5.I'll put the output image so you can see the color issue , i am not getting pure white its like a red/pink  tinted screen from my view

LVGL  ver-8.3.11

മീഡിയ (2).jpeg

മീഡിയ.jpeg

  the label is white and arc background color is grey, but this is what I am getting

1 REPLY 1
mƎALLEm
ST Employee

Hello, @b1aze 

LVGL is not a ST solution. Please ask that question in LVGL community: https://forum.lvgl.io/

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.