2026-05-20 8:44 AM
Hello,
ich set up my project with CubeMX for a CAN-FD (1 MBit/s / 4,8 MBit/s) and a Display for communication. Now i have the problem, that the SCK Signal for the communication looks more like a sawtooth signal than a rectangle. Also the SPI-Prescaler for the baud rate does not affect this signal. i am really confused. I need to use the 48 MHz HSE for my 4,8 MBit/s data phase for CAN-FD.
I use an NUCLEO-C092RC and a LCD Display with ILI9341 (library from Mauro De Vecchi)
Thanks for the help
2026-05-20 8:47 AM - edited 2026-05-20 8:48 AM
Hello,
Sorry your question is not clear.
How to write your question to maximize your chances to find a solution
Please focus on the problem and forget about the unnecessary info.