2010-08-18 6:27 AM
Hi all
I just wanted to flag a problem with the Rflasher and ST visual programmer regarding the chip ST72F521M9
Ride7: 7.30.10.0159
Rkit STM8 for ride 7 2.30.10.075
Ride 7 patch 7.30.10.169
=> The option byte calculated via those software are WRONG!
I figured out that by entering manually the hexadecimal option byte everything works eg:''27 87''
Hopefully this will be taken into account for the next release of the software...
Thanks for your time
Best regards
Rémi
2010-09-03 1:48 AM
Hi,
For Rflasher soft, it's Raisonance. Which version of STVP ? Download and install the latest, you have to choose ST72F521x9 on STVP and TQFP80 is the default package. The error is on which bit(s)? On Package bits? Rgds, Laurent