2005-10-06 11:28 PM
Who should I trust? Ref Book or str71x lib ?
2005-10-05 3:55 AM
I am working on the apb reset procedure, and I noticed that the ref book told us that Bit 0 refer to the I2C0 component.
But the apb.h defined : #define I2C0_Periph 0x0002 Who should I trust ? Ludo2005-10-05 4:05 AM
I think the datasheet is correct and the libraries are wrong.
I least this works for me. Only stopping clocks, not the reset bits.2005-10-06 3:28 AM
Could ST please confirm the findings above.
Regards sjo2005-10-06 11:28 PM
Hi all,
Sorry for the delay, After test we confirm that the reference manual is correct and the libraries must be corrected. Best regards, Hich