cancel
Showing results for 
Search instead for 
Did you mean: 

stpc atlas-disk on chip

jayashree
Associate II
Posted on October 07, 2005 at 12:04

stpc atlas-disk on chip

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jayashree
Associate II
Posted on October 05, 2005 at 05:15

hello,

in the evaluation board schematic the diskon chip 2000 is mapped to 4 different 8kB locations in the memory through various jumper settings.can you tell me why it is done so ?

kaouther
Associate II
Posted on October 07, 2005 at 12:04

These 4 memory loactaions corresponds to the 4 possibility of Memory address at which DiskOnChip will be located.

It is not mapped to the 4 adress at the same time. There are only 2 jumpers for memory adress configuration . So you have the possibility to select only one of the fourth configuration.