cancel
Showing results for 
Search instead for 
Did you mean: 

unable to get the device descriptor's description

raunaque
Associate II
Posted on October 27, 2004 at 11:39

unable to get the device descriptor's description

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
raunaque
Associate II
Posted on October 27, 2004 at 07:31

Hi

friends ,

There is a firmware having the USB libraries apart from the code . The firmware is successfully burnt on the device through the in- circuit programming . when i plug the device on my PC and try to see the device descriptor using a software all the fields of the device descriptor is zero . but it shows that the device is connected and bus powered.

i am not able to trace the fault

can any body take me out of this situation

waiting for the reply

Ronnie

alain2399
Associate II
Posted on October 27, 2004 at 11:39

In order to have answer fro UB experts you should post your question in the USB forum.