2004-10-27 2:39 AM
unable to get the device descriptor's description
2004-10-26 10:31 PM
Hi
friends , There is a firmware having the USB libraries apart from the code . The firmware is successfully burnt on the device through the in- circuit programming . when i plug the device on my PC and try to see the device descriptor using a software all the fields of the device descriptor is zero . but it shows that the device is connected and bus powered. i am not able to trace the fault can any body take me out of this situation waiting for the reply Ronnie2004-10-27 2:39 AM
In order to have answer fro UB experts you should post your question in the USB forum.