cancel
Showing results for 
Search instead for 
Did you mean: 

Timer0 Configuration Inaccuracy

paulsmitton9
Associate III
Posted on August 14, 2008 at 06:17

Timer0 Configuration Inaccuracy

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
paulsmitton9
Associate III
Posted on May 17, 2011 at 09:54

I am using Timer0 to overflow and interrupt every 10ms,

and toggling a port in the Interrupt (and clearing flag).

I am using the 25 MHz oscillator as the main clock,

and the APB clock is set to 25 MHz / 4 = 6.25 MHz.

I can achieve a timing of 10.00 ms with the following:

Code:

TIM_InitStructure.TIM_Prescaler = 25 - 1; // 6.25 mhz / 25 = 250 khz = 4 us period

TIM_InitStructure.TIM_Full_Period = 2500 - 1; // 4 us * 2500 = 10ms

However I get a timing of 10.14 ms with the following:

Code:

TIM_InitStructure.TIM_Prescaler = 250 - 1; // 6.25 mhz / 250 = 25 khz = 40 us period

TIM_InitStructure.TIM_Full_Period = 250 - 1; // 40 us * 250 = 10 ms

Please could someone explain why I get a discrepancy

of 0.14 milliseconds with the second configuration?

I am using STR912FW44X6 with no other peripherals on.

Thanks,

Paul.

paulsmitton9
Associate III
Posted on May 17, 2011 at 09:54

This forum seems quiet.

The discrepancy occurs because the counter resets to 0xFFFC,

rather than the assumed 0x0000, giving an extra four ticks.

In the first instance this causes an undetected 16us.

In the second instance this causes a 160us (0.16ms) difference.

chifoukalou
Associate II
Posted on May 17, 2011 at 09:54

Paul,

Is it part of normal behavior that timer resets to 0xFFFC or is it a silicon bug?

May I ask you what type of tool chain you are using and if you work with floating points (this has nothing to do with your post)?

Thank you in advance.

Joel

paulsmitton9
Associate III
Posted on May 17, 2011 at 09:54

Well it's intentional, although i've no idea why.

It's documented in the manual (e.g. figure 44).

I'm using idealist (with sarm) which is great.

I don't use floating point, fixed works fine :)

chifoukalou
Associate II
Posted on May 17, 2011 at 09:54

Thank you for your feedback, I will be carefull when using Timer (expected soon along my current design).

I also use Idealist which is the only tool chain I was able to use with floating point. With the other GCC tool chain (Yagarto, Crosswork, Ride,...) the result of printf with floating point was not succesfull. It is why I asked you this question.

Regards,

Joel

amira1
Associate II
Posted on May 17, 2011 at 09:54

Hello chifoukalou and all,

I wanted just to clarify that the reset value 0xFFFC of the timer counter is not a bug. However, it represents the spec of the STR9 TIM and it is well detailed in the reference manual to do not make confusion for our customer.

Best regards,

mirou.