Posted on May 17, 2011 at 09:54Thank you for your feedback, I will be carefull when using Timer (expected soon along my current design). I also use Idealist which is the only tool chain I was able to use with floating point. With the other GCC tool ...
Posted on May 17, 2011 at 09:54Paul, Is it part of normal behavior that timer resets to 0xFFFC or is it a silicon bug? May I ask you what type of tool chain you are using and if you work with floating points (this has nothing to do with your post)? ...
Posted on May 17, 2011 at 09:53There are two great tutorial to setup eclipse/yagarto: - ''Using Open Source Tools for AT91SAM7S Cross Development'' from James P.Lynch, - ''Using Open Source Tools for STR7xx Cross Development'' from G.A. Fazio et A.D...