2008-09-29 11:44 PM
STR912FW44: Data abort after 32k flash boundary (ADR 0x8000 and higher)
2011-05-17 2:32 AM
Hi guys,
I am writing a C low level startup sequence for the STR912FW44. As soon as the code tries to read flash memory past the 32k memory (address 0x8000 and higher) I get a data abort exception. Can anyone give me a hint of what I might be missing or doing wrong? Thanks! Pieter Here is my C initialisation code: void LowLevelInit(void) { /* ''Buffered'' is defined in ''91xconf.h'' */ #ifdef Buffered __asm__ __volatile__( ''mrc p15, 0, r0, c1, c0, 0 \n\t'' /* Read CP15 c1, Control Register */ ''orr r0, r0, #0x8 \n\t'' /* Enable BIU write buffer on AMBA AHB */ ''mcr p15, 0, r0, c1, c0, 0 \n\t'' /* Write CP15 c1, Control Register */ : : : ''r0''); #endif /* * Set bits 17 (Data TCM order bit) and bit 18 (Instruction TCM order bit) * in the Configuration Control Register. */ __asm__ __volatile__( ''mov r0, #0x60000 \n\t'' ''mcr p15, 1, r0, c15, c1, 0 \n\t'' : : : ''r0''); /* * Map Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000, * when the bank 0 is the boot bank, then enable the Bank 1. */ FMI->BBADR = 0x00000000>>2; /* Set Boot bank base address to 0x00000000 */ FMI->BBSR = 4; /* Set Boot bank size to 512KB */ FMI->NBBADR = 0x00080000>>2; /* Set Non boot bank base address to 0x00080000 */ FMI->NBBSR = 2; /* Set Non boot bank size to 32KB */ FMI->CR = 0x18; /* Enable Flash Boot Bank and Non Boot Bank */ /* Enable SRAM */ SCU->SCR0 = 0x187 | (2 << 3); /* Set System configuration register to 96K SRAM size */ }2011-05-17 2:32 AM
Sorry, wrong forum. I will repost in STR9
Regards, Pieter