2008-10-05 11:30 PM
2011-05-17 2:32 AM
Hello,
I want to use Ethernet port availabe on STr9 and interface my system using TCP / IP protocol. I searched for the ready code availabe on ST9 application notes , but i could not get implementation for TCP protocol for transport layer. all i got is either UDP or UIP. Has anyone tried to implement or got any sample source for TCP ? How difficult or complex it is to implement TCP protocol? Also i donnot know what exactly UIP protocol is ? Dose all or maximum applications ( TCP /IP) use UDP or UIP for transport layer ? Can anyone give me likes where i can get more details for TCP implementations ? regards, NN.2011-05-17 2:32 AM
sorry wrong forum..... i will post it in STR9