cancel
Showing results for 
Search instead for 
Did you mean: 

STR912FW44: Data abort after 32k flash boundary (ADR 0x8000 and higher)

pieter2399
Associate II
Posted on October 06, 2008 at 12:31

STR912FW44: Data abort after 32k flash boundary (ADR 0x8000 and higher)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
pieter2399
Associate II
Posted on May 17, 2011 at 09:56

Hi guys,

I am writing a C low level startup sequence for the STR912FW44. After the routine has finished, the code then tries to read flash memory past a 32k ''boundary'' (address 0x8000 and higher), e.g. address 0xa444, and a data abort exception is thrown.

The STR912FW44 has 512k flash mapped to bank 0 and 32k flash is mapped to bank 1. I am able to successfully program a 41k application into flash.

Can anyone give me a hint of what I might be missing or doing wrong?

Thanks!

Pieter

Here is my C initialisation code:

void LowLevelInit(void)

{

/* ''Buffered'' is defined in ''91xconf.h'' */

#ifdef Buffered

__asm__ __volatile__(

''mrc p15, 0, r0, c1, c0, 0 \n\t'' /* Read CP15 c1, Control Register */

''orr r0, r0, #0x8 \n\t'' /* Enable BIU write buffer on AMBA AHB */

''mcr p15, 0, r0, c1, c0, 0 \n\t'' /* Write CP15 c1, Control Register */

: : : ''r0'');

#endif

/*

* Set bits 17 (Data TCM order bit) and bit 18 (Instruction TCM order bit)

* in the Configuration Control Register.

*/

__asm__ __volatile__(

''mov r0, #0x60000 \n\t''

''mcr p15, 1, r0, c15, c1, 0 \n\t''

: : : ''r0'');

/*

* Map Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000,

* when the bank 0 is the boot bank, then enable the Bank 1.

*/

FMI->BBADR = 0x00000000>>2; /* Set Boot bank base address to 0x00000000 */

FMI->BBSR = 4; /* Set Boot bank size to 512KB */

FMI->NBBADR = 0x00080000>>2; /* Set Non boot bank base address to 0x00080000 */

FMI->NBBSR = 2; /* Set Non boot bank size to 32KB */

FMI->CR = 0x18; /* Enable Flash Boot Bank and Non Boot Bank */

/* Enable SRAM */

SCU->SCR0 = 0x187 | (2 << 3); /* Set System configuration register to 96K SRAM size */

}

dhoyen
Associate II
Posted on May 17, 2011 at 09:56

Hi pieter,

Here my init function, which do exactely what you are looking for:

I m using the Bank0 for startup-program and the bank1 for emulate EEPROM and keep some data. Both work correctly.

I use the lib. from ST.

You can take a look also on the other part of the code (commented #if 0), this code works, and don't use the ST lib.

Regards.

Damien

FMI_BankRemapConfig (0x04,0x02,0x00000000, 0x00080000);

//Arg 1 -> 0x4: Boot bank size 512KBytes.

//Arg 2 -> 0x2: Non Boot bank size 32KBytes.

//Arg 3 -> Mapping address boot bank

//Arg 4 -> Mapping address NON boot bank

/* Turn ON clock*/

SCU_FMICLKDivisorConfig(SCU_FMICLK_Div1);

//never put FMI in reset here, or will crash

SCU_AHBPeriphClockConfig(__FMI, ENABLE);

SCU_AHBPeriphReset(__FMI, DISABLE);

FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0, FMI_PWD_ENABLE,FMI_LVD_ENABLE, FMI_FREQ_HIGH);

#if 0

//previous code, from the STR912 GCC port from Richard Berry, FreeRTOS corp.

// For info only

FMI->BBSR = 4;

FMI->NBBSR = 2;

FMI->BBADR = (0 >> 2);

FMI->NBBADR = (0x80000 >> 2);

FMI->CR |= 0x18;

FMI->CR &= FMI_WRITE_WAIT_STATE_0;

*(vu16 *)FMI_BANK_1 = 0x60;

/* need 3 read wait states if operating @ 96Mhz */

*(vu16 *)(FMI_BANK_1 | FMI_READ_WAIT_STATE_3 | FMI_PWD_ENABLE | FMI_LVD_ENABLE | FMI_FREQ_HIGH) = 0x03;

#endif

pieter2399
Associate II
Posted on May 17, 2011 at 09:56

Hi Damien,

Thanks for the help!

It turns out that if DEBUG is defined in ''91xconf.h'' (or in my Makefile), the peripheral registers are declared as ''extern'' in ''91x_map.h'' and initialised to correct values in the function ''debug()'' in ''91x_lib.c''.

I did not call ''debug()'' first and my lowlevel C initialisation function accessed random values in stead of correct registers.

Regards,

Pieter