2007-09-09 8:26 PM
2011-05-17 12:46 AM
The CPU start ok with JTAG, but then I start it without JTAG it not works
seems to jump into ABT handler, the code is about 200K, any solutions ?2011-05-17 12:46 AM
Hi,
Could you precise which IDE are you using? Are you using St's startup files or your own startup file? Have a look to thishttp://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware
in order to get the last version. Regards, MBS [ This message was edited by: MBS on 21-08-2007 11:54 ]2011-05-17 12:46 AM
Hi
It works now, I was trying to change the clock from high to low for writing to Flash, and I found in Errata it is a problem to do that, so I take that away and use function i RAM instead to handling the Flash2011-05-17 12:46 AM
Hello JW,
Did you resolve your problem and if so what was it and what did you do to fix it ? Has anyone else had similar problem ? (And found a fix that they can share ?) I migrated my project to the IAR 5.1 compiler (using latest silicon - STR911 FA). The project runs with j-Trace plugged in, but not without it. Thanks, Rhys