2008-04-17 2:53 AM
STR9 Reset Himself during UART transmission
2011-05-17 12:52 AM
When tranmiting packet RX (From PC) and TX (To PC), after a moment (random), the CPU resets. I don't use the Watchdog. This happens either on the STR912FAW44X6 and 47X6. This is not a desired feature. What can happen there? Thanks
2011-05-17 12:52 AM
Hi,
have you tried to use the UART example delivered with STR9 software library available in ST web site, may be you have a software pb? Regards,2011-05-17 12:52 AM
Yes, it's sure that I have watch some exemple. The UART used to work properly. What can make the CPU resets?
2011-05-17 12:52 AM
It reset during the TX (the last packet before the reset is incomplete).