2007-11-27 6:35 PM
2011-05-17 2:31 AM
I'm using 91x_lib and I'm trying to write a simple application that use TIM and VIC interrupts. I haven't any examples, someone have examples?
This is my code that doesn't work: ***** main.c ****** #include ''91x_lib.h'' TIM_InitTypeDef TIM_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; void main(void) { #ifdef DEBUG debug(); #endif SCU_APBPeriphClockConfig(__VIC, ENABLE); /* Deinitialize the VIC */ VIC_DeInit(); SCU_APBPeriphClockConfig(__GPIO6, ENABLE); GPIO_DeInit(GPIO6); SCU_APBPeriphClockConfig(__GPIO3, ENABLE); GPIO_DeInit(GPIO3); SCU_APBPeriphClockConfig(__TIM01, ENABLE); TIM_DeInit(TIM0); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt1; GPIO_Init(GPIO6,&GPIO_InitStructure); /* GPIO4 configuration (PWM on P4.0 pin 3) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO3,&GPIO_InitStructure); /* TIM0 Structure Initialization */ TIM_StructInit(&TIM_InitStructure); /* TIM0 Configuration in PWM Mode */ TIM_InitStructure.TIM_Mode = TIM_PWM; TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB; TIM_InitStructure.TIM_Prescaler = 0xFF; TIM_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH; TIM_InitStructure.TIM_Period_Level = TIM_LOW; TIM_InitStructure.TIM_Pulse_Length_1 = 0x3FF; TIM_InitStructure.TIM_Full_Period = 0xFFF; TIM_Init (TIM0, &TIM_InitStructure); VIC_Config(TIM0_ITLine, VIC_IRQ, 0); VIC_ITCmd(TIM0_ITLine,ENABLE); TIM_ITConfig(TIM0,TIM_IT_IC1|TIM_IT_OC1|TIM_IT_TO|TIM_IT_IC2|TIM_IT_OC2,ENABLE); /* Start the counter of TIM0 */ TIM_CounterCmd(TIM0, TIM_START); while(1){ VIC_SWITCmd(TIM0_ITLine, ENABLE); } } ***** 91x_it.c *** .... void TIM0_IRQHandler(void) { GPIO_WriteBit(GPIO6, GPIO_Pin_All, Bit_RESET ); } ....2011-05-17 2:31 AM
Hi,
declare your IRQ function in it.c like this one, don't forget to change it.h : __irq void TIM0_IRQHandler(void) { ''Code'' // VIC re-init TIM_ClearFlag(TIM2, TIM_FLAG_TO); //TimerFlag clear VIC0->VAR = 0 ; //dummy for VIC0 Line VIC1->VAR = 0 ; //dummy for VIC1 Line } in VIC.C you must change the function static void VIC_ISRVectAddConfig(u16 VIC_Source, u16 VIC_Priority, void (*VIC_VectAddress); to: static void VIC_ISRVectAddConfig(u16 VIC_Source, u16 VIC_Priority, void (*VIC_VectAddress)(void)__irq);