2007-07-03 3:15 AM
2007-05-23 10:52 PM
Hi,
We have developed a board using a STR715. As it will run under battery in case of power failure, we have implemented the LPWFI mode (we also tried the STOP mode with the same result). When waiting for an event, the board uses 900µA. We expected 150µA maximum (processor + regulator + MAX3243 + HC4060 used as oscillator). Main oscillator (HC4060) is stopped, MAX3243 is powered down, regulator (LP2985 use 100µA for 1mA load), flash powered down, MVR off, running from RTC (32768Hz) Here is the code used to go into low power mode // stop external oscillator (activates the RST input to stop the oscillator) SetSHUTDOWN(); // deselect & reset PLL1 PRCCU_CFR&=0xFE; PRCCU_PLL1CR&=0xFFFFFF7F; PRCCU_PLL1CR|=0x7; // deselect & reset PLL2 (strange as PLL2 is not provided in STR715 but 1.4mA less current when done) PRCCU_PLL2CR&=0xFF7F; PRCCU_PLL2CR|=0x7; // select CKAF in LPWFI mode PRCCU_CCR|=0x0002; // select low power mode during WFI PRCCU_CCR|=0x0001; // stop flash during LPWFI mode FLASH_CR0|=0x8000; // disable MVR during LPWFI mode PRCCU_PWRCR|=0x8000; PRCCU_PWRCR|=0x0010; PRCCU_PWRCR&=0x7FFF; // activate LPWFI mode PRCCU_SMR&=0xFFFE; Any idea will be helpfull as it is very important to get the remaining 750µA Thanks for any answer2007-05-31 10:09 PM
Dear Marc,
Please make sure that you already selected the RTC clock prior switching off the oscillator using the SetSHUTDOWN() function? Once you switch off the main oscillator no need to switch to CLk2 clock, you can switch to PLL Free running mode instead. Could you test these steps; - Switch to RTC clock, - stop the main oscillator To further reduce power consumption, it is required to clear some bits in the RCCU_PER register as recommended in the STR71x reference manual. And also disable PLL2 as done. - select CKAF in LPWFI mode - stop flash during LPWFI mode - disable MVR during LPWFI mode Could you test the Stop mode if you still have the same power consumption as in LPWFI mode? Regards.2007-06-05 1:08 AM
Hello,
Thanks for your answer. This is exactly what I did. In a few days I will have a new prototype board so I will make some more tests with this one. In any case, I will retry also using the stop mode. I will inform you with the results of the new board. Regards.2007-07-03 3:15 AM
Hello,
With our final pcb, everything seems to be ok since now the board needs only 110µA in WFI mode. This value is the same for 99% of the production we tested until now. There was a problem with the programming of the I/O pins and this problem draw 300µA in excess. The last µA regained are due to the pcb and there is no explanation since the production is exactly the same as the prototype, except the prototype was soldered by hand. Regards