Posted on July 03, 2007 at 12:15Hello, With our final pcb, everything seems to be ok since now the board needs only 110µA in WFI mode. This value is the same for 99% of the production we tested until now. There was a problem with the programming of...
Posted on June 05, 2007 at 10:08Hello, Thanks for your answer. This is exactly what I did. In a few days I will have a new prototype board so I will make some more tests with this one. In any case, I will retry also using the stop mode. I will infor...
Posted on May 24, 2007 at 07:52Hi, We have developed a board using a STR715. As it will run under battery in case of power failure, we have implemented the LPWFI mode (we also tried the STOP mode with the same result). When waiting for an event, the...