2003-12-08 2:40 AM
2003-11-28 12:36 AM
Hi,
Sometimes my st7lite29 application doesn't start when i switch on the power. When i add a reset network (1µF cap to gound and 100 kohm to +5V) it works fine any time. It is absolutely no problem for me to add those two components, but i seem to be the only one who has to do this. Maybe i'm doing something wrong... Ex. is it necessary to switch on the LVD? Greets.2003-11-28 1:12 AM
Hello joble
according to datasheet p112, it is indeed necessary to use LVD, or a reset circuit. You are not the only one who does need it.2003-12-02 12:35 AM
What is the best solution, the LVD or the external RC-network?
The external RC seems to me the most reliable.2003-12-02 3:40 AM
Incase you use internal reset circuit(LVD), you will have to connnect 0.01 uf capacitor between GND and the reset pin.
2003-12-02 6:01 PM
I have done it with LVD, and it works fine! I never tried a reset-circuit because it is more expensive than LVD, and I never had any problem with the reliability of the LVD.
2003-12-08 12:22 AM
Ok, the LVD is totaly clear to me now. I'm going to remove the rc and use the lvd.
Just one more question: Is it ok to use the highest treshold voltage (4.1V) for a 5V supply. I suppose it is, but just want to be sure. Thanks!2003-12-08 2:40 AM
Yes, it is if you have a normaly filtered power supply. Maybe you should also use the AVD to safely shut down the mcu (depends on your application), before it is internally reset.