Posted on January 13, 2006 at 08:59Hi, while compiling a workspace for ST7DALI this error occurs: #error clnk Release\rgb_driver_dmx_v1_0.lkf:1 no default placement for segment .version #error clnk Release\rgb_driver_dmx_v1_0.lkf:1 no default placem...
Posted on September 28, 2005 at 09:30Is it possible to generate hardware PWM at a frequency of 1kHz with a 16MHz Xtall on an ST7LITE39? Fcpu = 16Mhz/2 = 8MHz so 2kHz PWM is the minimum. But what about the possibility to use the Lite Timer to clock t...
Posted on June 29, 2005 at 06:52Hi, Strange problem with an ST72F264G2: The program has worked completely, after minor changes it doesn't work anymore. This is what happens: When i enable interrupts (_asm(''_rim'')), the main progam stops. Only othe...