2007-06-11 8:58 PM
2007-06-11 4:19 AM
Hello!
Can somebody say to me, what's the typical resistance/impedance of an input pin at the ST7LITE39. I've been connected the PIN and declared as Floating-Input for the ADC (AIN3). I want to divide the voltage with a second resistor and need the exact value. Thank you. Best Regards, Heiko2007-06-11 7:22 PM
The replay to your question is in the section 13.8.2 ''I/O Port Pin Characteristics'' of ST7FLITE39 datasheet.
Please, be informed that the input resistance is not linear owing to the input protection diodes. In my opinion, to attenuate and feed an input signal to the ADC, it is better to attach the AIN3 pin to an external resistor series where flows a current of about 100uA so that the ADC leakage current (1uA) may be ignored. BR EtaPhi2007-06-11 8:58 PM
Hi,
thank you for the reply. I have been changed the configuration with the input divider of the resistors. Now I'll use a external resistor. I have been found the note in the users guide. Now it works well ;-). Regards, Heiko