Posted on June 12, 2007 at 05:58Hi, thank you for the reply. I have been changed the configuration with the input divider of the resistors. Now I'll use a external resistor. I have been found the note in the users guide. Now it works well ;-). Regar...
Posted on June 11, 2007 at 13:19Hello! Can somebody say to me, what's the typical resistance/impedance of an input pin at the ST7LITE39. I've been connected the PIN and declared as Floating-Input for the ADC (AIN3). I want to divide the voltage with...
Posted on June 01, 2007 at 05:44Hello together! I have a problem with the configuration with the oszillator setup. I want to start the MCU with 8Mhz on the fcpu. I need the Pll and the CPU voltage about 5VDC. The MCO will be enabled with 4 MHz. I wr...