2002-11-22 6:46 AM
ST7lite05 external clock connection?
2002-11-21 4:48 PM
I want to use a crystal oscillator in ST7lite05. But I don't know how to connect? Could you give me a hand?
Terry Hao terryhao@citiz.net2002-11-22 12:00 AM
ST7Flite0 has been specifically designed to be used with the embedded internal 1% RC. Therefore crystal isn't expected to be used with this device and no dedicated pins are available.
Feel free to use the internal RC + PLLx4x8 to reach your CPU frequency: 1, 4, or 8MHz. Pierre2002-11-22 6:46 AM
The lite05 cannot drive a crystal directly but can accept a logic CMOS level Clock. In this configuration you can either use an external clock chip or build your own using inverters.
I found the enclosed application note from Epson very useful for my own oscillator design. ________________ Attachments : O_D_guide.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I02K&d=%2Fa%2F0X0000000bU0%2FtuVXXrojKuDMr8.b5N0epK9VCsz8bgPNdzpgnVH6n1U&asPdf=false