2003-09-29 11:25 PM
2003-09-29 4:04 AM
Are thera any application notes about driving 7 segment displays?
Im using 2 shift registers (4094) and 4 x 7 segment displays.2003-09-29 11:25 PM
Hi,
It's a little old now, but look at the At the back ( around page 280 ), is a project using 4094's driving LCD's. I think the code to drive the 4094s is explained and/or included. You should be able to port this to the FLITE very easily. regards Simon