2005-07-14 7:59 PM
2005-07-10 2:11 AM
I would like to use the internal RC oscillator and also use SCI communication @4800baud.
I couldn't find in the datasheet the absolute min/max RC clock deviation between ST72264 devices. I would like to know if it's safe to use the internal RC without preforming calibration for each device? (the other timing beside the SCI communication is negligible). Thx2005-07-14 4:07 AM
In section 6.2 (Multi-Oscillator) of the datasheet, it indicates that the RC oscillator has lower frequency accuracy.
In section 13.5.4 (RC Oscillators), it indicates that the internal frequency can vary from 2 to 6 MHz. Since this is a factor of 3 difference, I'm not sure if there is much hope for any SCI communication without calibration through the Baud Rate registers and/or Extended Prescalers. It also looks like temperature can affect RC timing significantly, so you may want to make sure you are at operating temp before attempting calibration.2005-07-14 7:59 PM
Latino,
even if ST72264 devices SCI are not LIN compatible, you could follow what LIN protocol suggests to syncronize clocks. For instance, the sender may send a BREAK character whose duration is known. The ST2264 receiver could then measure this duration and set-up his local oscillator according to the result. Then, the only thing that matters is the clock short-term stability. I hope I was useful... EtaPhi