Posted on July 14, 2005 at 13:07In section 6.2 (Multi-Oscillator) of the datasheet, it indicates that the RC oscillator has lower frequency accuracy. In section 13.5.4 (RC Oscillators), it indicates that the internal frequency can vary from 2 to 6 M...
Posted on July 14, 2005 at 12:59I'm not sure about using an alternate function (output I'm guessing) in conjunction with an ICC interface. Every time I've had to share a pin with ICC, it has been used as an input to the MCU. When I use the Indart-ST...
Posted on June 24, 2005 at 13:01I am using the STVD 3.1.1 to simulate software that I have written for the ST72F264G2. This software makes use of pins on Port C and Port B for interrupt purposes. Each port needs to be on a different interrupt bank (...
Posted on February 24, 2005 at 11:22Thanks for the suggestions. I did make sure to write OCiHR first, followed by OCiLR (based on Note 1, page 66). Since I'm using interrupts, I also made sure to clear the interrupt based on ICF1 (Note 3, page 66) b...
Posted on February 23, 2005 at 14:10I am trying to work with the timer-based PWM on the ST72264 and have been having some problems. I think I may have figured out a solution (thanks to reading the messages on this forum), but I would like to see if ...