2006-04-11 2:30 AM
2006-04-11 2:30 AM
hello all,
i've problem triggering external interrupts and would like to confirm what've done wrong.. interrupt vectorvoid (* const _vectab[])() = { NULL, /* 0xFFE0 pwmart*/ NULL, /* 0xFFE2 i2c*/ it_AVD, /* 0xFFE4 avd*/ it_sci, /* 0xFFE6 sci*/ it_timeB, /* 0xFFE8 timerb*/ it_timeA, /* 0xFFEA timera*/ it_spi, /* 0xFFEC spi*/ CAN_Interrupt, /* 0xFFEE can*/ it_ei3, /* 0xFFF0 pb4..7*/ it_ei2, /* 0xFFF2 pb0..3*/ it_ei1, /* 0xFFF4 pf0..2*/ it_ei0, /* 0xFFF6 pa0..3*/ it_clock, /* 0xFFF8 mcc*/ NULL, /* 0xFFFA tli*/ it_trap, /* 0xfffc trap*/ _stext, /* 0xfffe main*/ }; cpu initialization/* pb0..3 = outputs pb4..6 = digital inputs (encoder) pb7 = output */ PBDR = 0x80; PBDDR = 0x8f; PBOR = 0x8f; EICR = 0x40; i'd like to use pb4 and pb5 for encoder input for both channels, and i need to have external interrupt 3 triggered on any edge of these inputs. interrupt routine@interrupt void it_ei3(void) { encoder.extint++; // increase debug counter if ((!(encoder.olda & BIT4)) && (PBDR & BIT4)) { // a rising edge if (!(PBDR & DIN5)) encoder.counter++; // increase counter else encoder.counter--; // decrease counter } encoder.olda = (PBDR); // store old state } In above, encoder is volatile structure, and even the counter value is not changed, also the debug counter does not count - which means that external interrupt is never triggered. I just cannot figure out what's wrong with these settings. Please help!