2010-03-28 04:11 AM
I have upgraded my PC OS to win7 64bit. The Winee is not installabel on this OS. I have tried to install using the virtual XP mode, the program runs, but it can not communicate with my ST626x starter kit. LPT port are set to enhanced - two way.
Is there a way to overcome this problem? Is there another program/programmer I can use?2010-03-31 04:05 AM
I have installed ''VMware Workstation'', and XP mode. Winee installed to VMware in XP mode, runs ok. But it is 'payware'.