2006-02-22 10:29 PM
2006-02-16 8:12 PM
Hello!
According to manual on ST10F269 MAC unit, command coMOV can be used for data transfer to the entire memory space: ''The GPR pointer allows access to the entire memory space, but IDXi are limited to the internal Dual-Port RAM, except for the CoMOV instruction.'' (ST10F269 User's manual, rel1.2, page 62) My questions is: Does ''entire memory space'' means total 16-Mbytes range? How can I do it? All these registers are 16-bit wide, so I suppose, that additional registers also should be used as page registers ?2006-02-21 2:03 AM
Neila, thank you for yor reply!
I know about DPP0...DPP3 registers, but it is not clear for me, how to use them together with MAC registers. There is another way to get access to any memory location: extp R12,#1 mov [R10],R1 , for example. For me, it is also not clear, should I use similar sequence, like extp R12,#1 coMOV [IDX0+],[R11+] , when I use MAC registers? Is it possible to get some examples, where this issue described more detailed? Thanks in advance, Shandy