2007-10-31 1:48 AM
2007-10-30 9:44 PM
Hi all,
I have a question about ST10 user stack. In my linker file, I located it at 0xF0100, size 0x2000; so from 0xF0100 to 0xF20FF In my startup file, I can see the user stack init : MOV R0,#DPP2:?C_USERSTKTOP ... but since R0 is a 16 bit register, the value may be truncated... When I run the simulator, after this MOV instruction, the updated R0 value is 0xA100... My target works fine but I can't understand this 0xA100 value. Could you explain me ? Thanks a lot ! Pierre PS : I am using a ST10F276 [ This message was edited by: pierre.roth on 31-10-2007 10:20 ]2007-10-31 1:48 AM
OK I found an explanation about DPP registers.
User stack is located in NEAR memory which is accessed using DDP2. Therefore I think my R0 value is understandable : Stack located from 0xF0100 to 0xF20FF. R0 Value : Hex : A 1 0 0 Bin : 1010 0001 0000 0000 so DPP is 10 (bit 15-14) which is DDP2. DPP2 contains 0x3C and 0x3C * 4 = 0xF0 !!